If there are two or more events set for the trace start event, collection of trace data can be made to start when the trace start event satisfies the following combination conditions.
Also, if there are two or more events set for the trace end event, collection of trace data is finished when the condition for any one of trace end events is met.
To edit a set trace event, choose [Event] from the [View] menu, select the trace event on the Events panel that is opened, and then click [Edit Condition ...] on the context menu.
Do your editing in a dialog box that is opened by this operation.
For details on how to edit in a dialog box, see “2.17.4.3 Editing combination conditions of events [E1] [E20] [EZ Emulator]”.
Also see Cautions of "(1) Editing the combination condition" for details on combination conditions. |