2.13.3.3 Executing the program

Execute the program (see "2.9 Execute Programs").

Collection of trace data is started or finished when the condition set for a trace start event or trace end event is met.

For details on how to check the collected trace data, see “2.13.6 Displaying an execution history".