2.22.10 Lock bits [For microcontrollers with lock bits]

(1)

Clearing the lock bit before downloading

If the user program is to be downloaded into a flash ROM area for which a lock bit is set, E1/E20/EZ Emulator clears the lock bit of the block that contains download data before it starts downloading.

(2)

Restoring the lock bit after downloading

The behavior of the emulator depends on the setting of the [Debug the program re-writing the on-chip PROGRAM ROM] property in the [System] [E1] [E20] [EZ Emulator] category on the [Debug Tool Settings] tab of the Property panel.

<1>

[Yes]:

The lock bits are restored after downloading.

<2>

[No]:

The lock bits remain cleared even after downloading.