When either of the following conditions is met or when both of them are met,
An address in the microcontroller's on-chip flash ROM is specified as the origin of a DMAC or DTC transfer |
An address in the microcontroller's on-chip flash ROM is specified as the interrupt vector for a DMAC or DTC activation source or the DTC vector table |
do not perform any of the following operations if a DMAC or DTC request may be generated while the user program is stopped.
Writing to the microcontroller's internal flash ROM area from the Memory panel or Python console panel |