2.2 Uninstalling Real-time OS Package

You can uninstall real-time OS package using the CS+ Uninstaller.



From the Windows [Start] menu, select [Programs] >> [Renesas Electronics CS+] >> [CS+ Uninstaller]. The uninstallation begins.

Figure 2-2. CS+ Uninstaller Window



The CS+ Uninstaller window looks up all CS+ products and real-time OS package products you have installed, and displays them in a list of check boxes.

Click [Select all] to select all the check boxes.

Click [Unselect all] to clear all the check boxes.

Click [Uninstall] to uninstall the selected products.

Caution If all products are uninstalled, the CS+ Uninstaller will be also uninstalled automatically.

Remark See "CS+ Start" for details.