2.3 Create a Project for RI Series

The creation of a project for RI series is performed with the Create Project dialog box (See the CS+ Start "2.6.2 Create a new project").

From the [Project] menu, select [Create New Project...], the following dialog box will open.

Figure 2-3. Create Project Dialog Box



Select the item below on [Kind of project].

- Application(RI series name, Build tool name)

Select this to generate a project for RI series.