2.8 Start Task Analyzer Tool [RI78V4 V2.xx.xx][RI850V4 V2.xx.xx][RI600V4]
From [View] menu, select [Realtime OS] >> [Task Analyzer 1] or [Task Analyzer 2]. The Realtime OS Task Analyzer panel opens.
Figure 2-6. [Task Analyzer] Item
Figure 2-7. Realtime OS Task Analyzer Panel
Remarks 1. Up to two panels can be opened by the task analyzer tool: the Realtime OS Task Analyzer1 panel and the Realtime OS Task Analyzer2 panel.
2. See "RI78V4 V2
.xx.xx/RI850V4 V2.
xx.
xx/RI600V4 Analysis" for details.