20.13	 Data Queue Information (dataqueue[])
 Here, each data queue is defined.
 
 Parentheses < >show the user input part. 
 
 -	 Description
Define the data queue ID number.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to 255
 
 -	 When omitting
The cfg600px assigns the ID number automatically.
 
 -	 Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
 
 #define   <ID name>   <ID number>
 -	 Definition format
Symbol
 
 -	 When omitting
Cannot be omitted.
 
 3 )	 Data count (
buffer_size)
 
 -	 Description
Define the number of data that the data queue can be stored.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 0 to 65535
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 0) applied.
 
 4 )	 Wait queue attribute (
wait_queue)
 
 -	 Description
Define the wait queue attribute for sending.
Note, task wait queue for receiving is managed in FIFO order.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 TA_TPRI:	Task current priority order
Among tasks with the same current priority, they are queued in FIFO order.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: "TA_TFIFO") applied.