20.14	 Mailbox Information (mailbox[])
 Here, each mailbox is defined.
 
 Parentheses < >show the user input part. 
 
 -	 Description
Define the mailbox ID number.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to 255
 
 -	 When omitting
The cfg600px assigns the ID number automatically.
 
 -	 Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
 
 #define   <ID name>   <ID number>
 -	 Definition format
Symbol
 
 -	 When omitting
Cannot be omitted.
 
 3 )	 Wait queue attribute (
wait_queue)
 
 -	 Description
Define the wait queue attribute.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 TA_TPRI:	Task current priority order
Among tasks with the same current priority, they are queued in FIFO order.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: TA_TFIFO) applied.
 
 4 )	 Message queue attribute (
message_queue)
 
 -	 Description
Define the message queue attribute.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 TA_MFIFO:	The order of the message transmission request.
 
 TA_MPRI:	Message priority order
 
 -	 When omitting
The set value in the default system configuration file (factory setting: TA_MFIFO) applied.
 
 5 )	 Maximum message priority (
max_pri)
 
 -	 Description
When TA_MPRI is specified for 
message_queue, the message priority from 1 to 
max_pri can be used.
When TA_MFIFO is specified for 
message_queue, this item is only disregarded.
 
 -	 Definition format
Numeric value
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 1) applied.