20.12	 Eventflag Information (flag[])
 Here, each semaphore is defined.
 
 Parentheses < >show the user input part. 
 
 -	 Description
Define the eventflag ID number.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to 255
 
 -	 When omitting
The cfg600px assigns the ID number automatically.
 
 -	 Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
 
 #define   <ID name>   <ID number>
 -	 Definition format
Symbol
 
 -	 When omitting
Cannot be omitted.
 
 3 )	 Initial bit pattern (
initial_pattern)
 
 -	 Description
Define the initial bit pattern 
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 0 to 0xFFFFFFFF
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 0) applied.
 
 4 )	 Multiple wait permission attribute (
wait_multi)
 
 -	 Description
Define the attribute regarding whether multiple tasks are permitted to wait for the eventflag.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 TA_WSGL:	Not permit multiple tasks to wait for the eventflag.
 
 TA_WMUL:	Permit multiple tasks to wait for the eventflag.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: "TA_WSGL") applied.
 
 5 )	 Clear attribute (
clear_attribute)
 
 -	 Description
Define the clear attribute (TA_CLR).
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 NO:	Not specify the TA_CLR attribute.
 
 YES:	Specify the TA_CLR attribute.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: NO) applied.
 
 6 )	 Wait queue attribute (
wait_queue)
 
 -	 Description
Define the wait queue attribute.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following: However, when the TA_CLR attribute is not specified, the wait queue is managed in the FIFO order even if TA_TPRI is specified for 
wait_queue. This behavior falls outside 
mITRON4.0 specification.
 
 TA_TPRI:	Task current priority order
Among tasks with the same current priority, they are queued in FIFO order.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: TA_TFIFO) applied.