2.15.7.2 Event types that can be set and deleted during execution

Types of events that can be set or removed during execution of the program or during execution of the tracer/timer are described below.

The meaning of each mark in the table below is as follows:

 

Possible

 

Possible, if the program execution is allowed to pause for events
(Property panel >> [Debug Tool Settings] tab >> [Set Event While Running] category >> [Set event by stopping execution momentarily] property >> [Yes])

 

Impossible while tracer or timer is executing

-

Impossible, or not supported

Table 2.21

Event Types That Can be Set and Deleted during Execution

Event Type

Debug Tool to Use

IECUBE

E1/E20/EZ Emulator

Simulator

Without OCD Trace Function

With OCD Trace Function

8-bit bus width products

Except for 8-bit bus width products

Hardware Break
(before execution)

 

-

-

-

 

Hardware Break
(after execution)

 

 

 

 

 

Hardware Break
(access)

 

-

 

 

 

Software Break

 

-

-

-

-

Trace
(trace start/trace end)

 

-

-

-

-

Point Trace

 

-

-

-

-

Timer Result
(timer start/timer end)

 

-

-

-

-

Action (Printf)

 

-

-

-

-