Events do not occur during step execution (including return execution) and program execution by selecting [Go to Here] from the context menu. |
If the location set for an existing event changes to midway in an instruction because the program to debug has been downloaded again, re-set the event using the following method. |
If debugging information is available: |
If debugging information is not available: |
If a change to internal ROM/RAM changes the location the event is set to a non-mapped area, then set events will not occur (they will also not change to Invalid state /Suspended State on the Events panel). |
If you differentiate function or variable names by leading underscores, then CS+ may misrecognize them, and convert symbols or make break event settings invalid. This applies for cases like when you have two functions, one named "_reset" and the other named "__reset". |
If there is code (text sections) to be ROMified, any software break event set for that code will be deleted during copy to RAM. For this reason, no break will occur. |
[Simulator] |
For other than [IECUBE] |
For other than [Simulator] |