3.2.11 I/O ports

Below is a list of API functions output by the Code Generator for I/O ports use.

Table 3.11

API Functions: [I/O Ports]

API Function Name

Function

R_PORT_Create

Performs initialization necessary to control the I/O ports.

R_PORT_Create_UserInit

Performs user-defined initialization relating to the I/O ports.