r_undefined_exception


Performs processing in response to the undefined instruction exception.

Remark

This API function is called to run interrupt processing in response to an undefined instruction exception occurred when detecting the undefined instruction (unimplemented instruction) execution.

[Syntax]

void    r_undefined_exception ( void );

[Argument(s)]

None.

[Return value]

None.