Performs processing in response to the privileged instruction exception.
Remark | This API function is called to run interrupt processing in response to a privilegedundefined instruction exception occurred when detecting the execution of a privileged instruction in user mode. |
[Syntax]
void r_privileged_exception ( void );
|
[Argument(s)]
None.
[Return value]