r_floatingpoint_exception


Performs processing in response to the floating-point exception.

Remark

This API function is called to run interrupt processing in response to a floating-point exception occurred when detecting the five exception events ( overflow, underflow, inexact, division-by-zero, and invalid operation ) specified in the IEEE754 standard and another floating-point exception that is generated on detection of unimplemented processing.

[Syntax]

void    r_floatingpoint_exception ( void );

[Argument(s)]

None.

[Return value]

None.