< Compile Options / Microcontroller Options >
The default for this option is endian=little.
The endian type can also be specified by the #pragma endian extension. If both this option and a #pragma extension are specified, the #pragma specification takes priority. |