< Compile Options / Microcontroller Options >
The default for this option is to process the enumeration type size as the signed long type.
This option processes the enumerated data qualified by enum as the minimum data type with which the enumeration value can fit in.  | 
*1) When the -int_to_short option has been selected, the signed 4-byte integer type will be selected.