< Compile Options / Microcontroller Options >
[Format]
-bit_order = { left | right }
 | 
 
 
The default for this option is bit_order=right.
[Description]
-  | This option specifies the order of bit-field members.  | 
 
-  | When bit_order=left is specified, members are allocated from the upper bit.  | 
 
-  | When bit_order=right is specified, members are allocated from the lower bit.  | 
 
-  | The order of bit-field members can also be specified by the #pragma bit_order extension. If both this option and a #pragma extension are specified, the #pragma specification takes priority.  |