2.13.5.1 To temporarily stop collection of execution history

By selecting [Stop Trace] from the context menu on the Trace panel during program execution, it is possible to temporarily stop collection of trace data.

Use this feature when you want to stop only the trace function without halting the program and check the trace data that has been collected until you stop it.