This function sets conditions of a pseudo-error and runs a program. [RH850][E1/E2/E20/Full-spec emulator]
Specify conditions of a pseudo-error as a list. See the PseudoErrorCondition class for details. |
||
If pseudo-error conditions were set and the program was executed successfully: True
If there was an error when setting pseudo-error conditions and executing the program: False
This function sets conditions of a pseudo-error and runs a program according to the contents specified with PseudoErrorCondition[]. |
If both Name and BitName are set as conditions of a pseudo-error, Name is given priority and BitName is ignored. |