Renesas Electronics
debugger.Trace.Clear
This function clears the trace memory.
Remark
This function provides the same function as debugger.XTrace.Clear.
[Specification format]
debugger.Trace.Clear()
[Argument(s)]
None
[Return value]
If the trace memory was cleared successfully: True
If there was an error when clearing the trace memory: False
[Detailed description]
-
[Example of use]
>>>debugger.Trace.Clear()
False
>>>