This function deletes a conditional trace.
[Specification format]
debugger.Trace.Delete(timerNumber = "")
|
[Argument(s)]
|
|
|
|
timerNumber
|
Specify the trace event number to delete.
|
[Return value]
If a trace was deleted successfully: True
If there was an error when deleting a trace: False
[Detailed description]
- | This function deletes the trace of the trace event number specified by tracenumber. |
- | If traceNumber is not specified, then traces of all trace event numbers will be deleted. |
[Example of use]
>>>debugger.Trace.Delete(1)
True
>>>
|