|  |  |  | 
| 
E0592001 | 
Multiple input files are not allowed. | 
Only one input file can be specified. 
Use the list file to specify multiple input files. | 
| 
E0592002 | 
The option option cannot have an argument. | 
An argument was specified for an option that should not have arguments. | 
| 
E0592003 | 
The option option requires an argument. | 
No argument was specified in an option that requires arguments. | 
| 
E0592004 | 
The option option is specified more than once. | 
Only one option can be specified at one time. | 
| 
E0592005 | 
Requires an output file. | 
The output file corresponding to the input file was not specified.  | 
| 
E0592006 | 
Failed to read an input file file. | 
The folder name or file name may be incorrect. If the next file is specified in the list file, conversion of that file will start. | 
| 
E0592007 | 
Failed to write a result of conversion file file. | 
The folder name may be incorrect. | 
| 
E0592008 | 
Failed to write an output file file. | 
The folder name may be incorrect. | 
| 
E0592009 | 
Failed to read a list file file. | 
The folder name may be incorrect. | 
| 
E0592010 | 
Syntax errors in list file file. | 
The description of the list file is not correct. | 
| 
E0592011 | 
File name is corrupted. | 
There are duplicate file names among the input file, output file, and conversion result output file. | 
| 
E0592012 | 
Invalid file name. | 
Either the input file name specified on the command line or an input or output file name specified in the list file has exceeded 260 characters. | 
| 
E0592013 | 
Invalid argument for the option option. | 
The argument specification is invalid or the specified file name has exceeded 260 characters. | 
| 
E0592101 | 
Illegal syntax in string. | 
Conversion could not be performed because there was a syntax that is not allowed in the CA78K0. Modify the input file. | 
| 
E0592102 | 
Can not add inline function for assembly. | 
The number of inline functions for assembly has exceeded the upper limit. Modify the input file. | 
| 
E0592103 | 
Failed to delete a temporary file. | 
Deletion of a temporary file has failed. Delete the temporary file. |