|  |  |  | 
| 
W0592051 | 
Input file specified on the command line is ignored when the "-l" option is specified. | 
When the list file is specified, an input file cannot be specified on the command line at the same time. The list file specified by the "-l" option is converted and the input file is ignored. | 
| 
W0592052 | 
The "-c" option specified on the command line is ignored when it does not match the specification in list file (file). | 
The "-c" option specification corresponding to the input file "file" specified in the list file differs between the list file and command line. Conversion is performed in accordance with the specification in the list file. | 
| 
W0592053 | 
Invalid option option. | 
An invalid option was specified. 
Ignore the option. | 
| 
W0592054 | 
Invalid argument for the option option. | 
The argument specified in the "option" option is invalid. 
If the argument of the "-c" option is invalid, processing is performed with the default specification. | 
| 
W0592055 | 
Requires an input file. | 
The list file specified by the "-l" option is missing an input file specification. | 
| 
W0592151 | 
String cannot be changed to syntax of CC-RL. | 
string could not be changed to the CC-RL format. Modify the input file. |