|  |  |  |  | 
| 
M0592111 | 
Change | 
String1 was converted into string2. | 
The token was converted. | 
| 
M0592112 | 
Change | 
Bit access of I/O register was converted into macro call. | 
Since the bit access method of SFRs differs between the CA78K0 and CC-RL, the method is changed to make access using a macro. | 
| 
M0592113 | 
Change | 
'String' has been changed to syntax of CC-RL. | 
Since the description format differs between the CA78K0 and CC-RL, the description format is changed to that of the CC-RL. | 
| 
M0592121 | 
Insert | 
Inserted macro definition for bit access of I/O register. | 
Since the bit access method of SFRs differs between the CA78K0 and CC-RL, the method is changed to make access using a macro. | 
| 
M0592122 | 
Insert | 
Inserted #pragma interrupt NO_VECT. | 
#pragma interrupt without the vector table specification was generated. | 
| 
M0592123 | 
Insert | 
Inserted string. | 
A description in accordance with the CC-RL format was added. | 
| 
M0592124 | 
Insert | 
Add inline function string for assembly. | 
An inline function for assembly was generated. | 
| 
M0592125 | 
Insert | 
Inserted #pragma rtos_interrupt NO_VECT. | 
#pragma rtos_interrupt without the vector table specification was generated. | 
| 
M0592131 | 
Delete | 
String was deleted. | 
The description format is not available in the CC-RL. The description was deleted. | 
| 
M0592142 | 
Info | 
The section can not be converted. Because there is no matched section. | 
The section could not be converted because there is no corresponding section in the CC-RL. | 
| 
M0592143 | 
Info | 
Delete "AT start address". | 
This was deleted because an address cannot be specified by #pragma section in the CC-RL. | 
| 
M0592144 | 
Info | 
The MACRO cannot be converted. Because there is no matched macro. | 
The macro could not be converted because there is no corresponding macro in the CC-RL. | 
| 
M0592145 | 
Info | 
The label detected in the assembly code. Please correct label to appropriate content. | 
Only local labels can be written in an assembly-language function in the CC-RL. Modify the label to have suitable contents. | 
| 
M0592146 | 
Info | 
The language specification is dependent on 78K0. | 
The code needs to be reviewed when the device is changed from 78K0 to RL78. The code should be manually modified. |