R_ADC_Get_Result_8bit

Reads the results of A/D conversion (8 bits; most significant 8 bits of 10-bit resolution).

[Syntax]

#include r_cg_macrodriver.h

void R_ADC_Get_Result ( uint8_t * const buffer);

[Argument(s)]

I/O

Argument

Description

O

Uint8_t * const buffer;

Pointer to area in which to store the results of A/D conversion

Remark Below is an example of the results of A/D conversion to be stored in buffer.


[Return value]

None.