R_ADC_Set_TestChannel

Sets the operation mode of A/D converter.

[Syntax]

#include r_cg_macrodriver.h

#include r_cg_adc.h

MD_STATUS R_ADC_Set_TestChannel ( test_channel_t channel );

[Argument(s)]

I/O

Argument

Description

I

test_channel_t channel;

Operation mode of A/D converter

ADNORMALINPUT: Normal mode (Normal A/D conver-

sion)

ADNORMALINPUT: Test mode (AVREFM input)

ADNORMALINPUT: Test mode (AVREFP input)

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification