Below is a list of API functions output by the Code Generator for A/D converter use.
Table 3.22 API Functions: [A/D Converter]
| 
 API Function Name  | 
 Function  | 
| 
 Performs initialization necessary to control the A/D converter.  | |
| 
 Performs user-defined initialization relating to the A/D converter.  | |
| 
 Performs processing in response to the A/D conversion end interrupt INTAD.  | |
| 
 Enables operation of voltage converter.  | |
| 
 Disables operation of voltage converter.  | |
| 
 Starts A/D conversion.  | |
| 
 Ends A/D conversion.  | |
| 
 Reset A/D conversion.  | |
| 
 Halts the clock supplied to the A/D converter.  | |
| 
 Configures the analog voltage input pin for A/D conversion.  | |
| 
 Enables the switch from STOP mode to SNOOZE mode.  | |
| 
 Disables the switch from STOP mode to SNOOZE mode.  | |
| 
 Sets the operation mode of A/D converter.  | |
| 
 Reads the results of A/D conversion (10 bits).  | |
| 
 Reads the results of A/D conversion (10 bits).  |