r_mac32bit_interrupt_flow

Performs processing in response to the 32-bit Multiply-accumulator interrupt INTMACLOF.

Remark This API function is called as the interrupt process corresponding to the 32-bit Multiply-accumulator interrupt INTMACLOF.

[Syntax]

CA78K0R Compiler

__interrupt static void r_mac32bit_interrupt_flow ( void );

CC-RL Compiler

static void __near r_mac32bit_interrupt_flow ( void );

[Argument(s)]

None.

[Return value]

None.