R_MAC32Bit_MACUnsigned

Operates the unsigned multiply-accumulate.

[Syntax]

#include r_cg_macrodriver.h

#include r_cg_mac32bit.h

void R_MAC32Bit_MACUnsigned ( uint32_t data_a, uint32_t data_b, mac32bit_uint64_t

* buffer_64bit );

[Argument(s)]

I/O

Argument

Description

I

uint32_t data_a;

Multiplicand

I

uint32_t data_b;

Multiplier

O

mac32bit_uint64_t * buffer_64bit;

Accumulation initial value Multiplier result

Remark See R_MAC32Bit_MULUnsigned for details about the mac32bit_uint64_t.

[Return value]

None.