R_MAC32Bit_Set_PowerOff

Stops the cock supplied for the 32-bit Multiply-accumulator.

Remark 32-bit Multiply-accumulator enters the reset state by calling this API.Therefore, writing to the registers which control 32-bit Multiply-accumulator is ignored after calling this API.

[Syntax]

void R_MAC32Bit_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.