R_TMR_KBm_BatchOverwriteRequestOn

Enables batch overwriting of the compare register.

Remark The timing for batch-overwriting the content of the compare register is when a count value and a value set in the compare register are matched or an external trigger is generated after calling this API function.

[Syntax]

void R_TMR_KBm_BatchOverwritRequestOn ( void );

Remark m is the unit number.

[Argument(s)]

None.

[Return value]

None.