R_TMR_KBm_ForcedOutput_mn_Start

Enables input of the trigger signal used for the forced output stop function.

[Syntax]

void R_TMR_KBm_ForcedOurput_mn_Start ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.