R_TMR_KBm_ForcedOutput_mn_Stop

Disables input of the trigger signal used for the forced output stop function.

[Syntax]

void R_TMR_KBm_ForcedOutput_mn_Stop ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.