Below is a list of API functions output by the Code Generator for 8-bit interval timer use.
Table 3.17 API Functions: [8-Bit Interval Timer]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 8-bit interval timer. | |
|
Performs user-defined initialization relating to the 8-bit interval timer. | |
|
Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1. | |
|
Starts the count of the 8-bit interval timer. | |
|
Ends the count of the 8-bit interval timer. | |
|
Halts the clock supplied to the 8-bit interval timer. | |
|
Halts the clock supplied to the 8-bit interval timer. |