This option specifies information that is output to the list file.
See "3.2 Link Map File" and "3.4 Library List File" for details about output information. |
To output the symbol address, size, type, optimization contents, and number of symbol references, describe as: |
The following table shows whether output information info will be valid or invalid by the combinations of the -form option and the -show or -show=all option. |
If a load module file, Intel Hex file, or Motorola S-record file is input, this combination will be invalid. |
The limitations on the output of the cross reference information are shown below.