Renesas Electronics
top
Compiler
CAUTIONS
Cautions Regarding Library and Startup
11.2 Cautions Regarding Library and Startup
This section explains the cautions regarding the library and startup.
Differences Information
Previous Topic
Controlling the Output of Bit Manipulation Instructions
Next Topic
Setting of Processor Mode Control Register (PMC)
Table of Contents
Cautions Regarding Compiler
Cautions Regarding Library and Startup
Setting of Processor Mode Control Register (PMC)
Label whose value is determined by the linker
Options necessary at assembling the startup file
Usage Restriction of Standard Library Function Name
Error in standard library functions
Definition of comparison functions bsearch and qsort in K&R format
Initialization of Stack Area at Startup
Specifying standard library functions when C99 standard is specified by an individual option
Cautions Regarding Assembler
Cautions Regarding Linker