11.2.2 Label whose value is determined by the linker

When the following labels used at startup are defined, operation becomes erroneous. Since the optimizing linker will determine these labels, definitions are unnecessary.

__STACK_ADDR_START, __STACK_ADDR_END, __RAM_ADDR_START, __RAM_ADDR_END