11.2.3 Options necessary at assembling the startup file

When startup is directly assembled without intervening the compiler driver, specify the following options.

-define=__RENESAS_VERSION__=0x01000000 ; When CC-RL V1.00 is used

-define=__RENESAS_VERSION__=0x01010000 ; When CC-RL V1.01 is used