< Compile Options / Source Options >
This option includes the specified file contents at the head of the compiling unit. Multiple file names can be specified by separating them with a comma (,). |
If there is more than one folder specified by the preinclude option, search is performed in turn starting from the leftmost folder. |