-ignore_files_misra [Professional Edition only]
|
< Compile Options / Source Options >
[Format]
-ignore_files_misra=<filename>[,<filename>,...]
|
[Description]
- | This option selects source files that will not be checked against the MISRA-C:2004 rules or MISRA-C:2012 rules. |
[Remarks]
- | If the option is specified more than once in the command line, all specifications are valid. |
- | This option is ignored when the misra2004 or misra2012 option has not been specified. |
- | <filename> is ignored when the specified file is not to be compiled. |