< Compile Options / Microcontroller Options >
[Format]
When -unsigned_char is omitted, char type values are handled as unsigned.
[Description]
- | When -unsigned_char is specified, char type values are handled as unsigned. |
[Remarks]
- | The bit-field members of the char type are not controlled by this option; control them using the signed_bitfield and unsigned_bitfield options. |