< Compile Options / Microcontroller Options >
The boundary alignment value for structures and classes equals the maximum boundary alignment value for members.
The boundary alignment value for structure members can also be specified by the #pragma pack extension. If both this option and a #pragma extension are specified, the #pragma specification takes priority. The boundary alignment value for structures and classes equals the maximum boundary alignment value for members. |
The boundary alignment values for structure members and class members when these options are specified are shown in the following table. |
Boundary Alignment Values for Structure Members and Class Members When the pack Option is Specified |