-outcode


< Compile Options / Other Options >

[Format]

-outcode = { euc | sjis | utf8 | big5 | gb2312 }

 

-

[Default]

The default for this option is outcode=sjis.

[Description]

-

This option specifies the character code to output characters in strings and character constants.

-

The options correspond to the character codes as shown in the following table.

Table 2.11

Correspondences between Options and Character Codes (outcode)

Option

Character Code

euc

EUC code

sjis

SJIS code

utf8

UTF-8 code

big5

Big5 code

gb2312

GB2312 code

 

[Remarks]

-

When outcode=big5 or outcode=gb2312, the big5 or gb2312 option must also be specified.