When the subcommand option is specified, the compiler options specified in a subcommand file are used at compiler startup. Specify options in a subcommand file in the same format as in the command line.
[Remarks]
-
If this option is specified for more than one time, all specified subcommand files are valid.