Renesas Electronics
-nodebug
< Assembler Command Options / Object Options >
[Format]
-
[Default]
If this option is not specified, no debugging information is output to the relocatable file.
[Description]
When the nodebug option is specified, no debugging information is output to the relocatable file.