-fpu


< Assembler Command Options / Object Options >

[Format]

-fpu

 

-

[Default]

The default for this option is fpu when the Instruction-code set as the ISA *1.

The default for this option is nofpu (when RX200 is selected as the target CPU *2) or fpu (in other cases).

Note

*1) This means a selection by the -isa option or the ISA_RX environment variable.

*2) This means a selection by the -cpu option or the CPU_RX environment variable.

[Description]

-

This option is used to generate a relocatable file which is capable of containing FPU instructions.

[Remarks]

-

Specifying fpu will lead to an error when the RX200 is selected as the target CPU.

-

For details of the FPU instructions, refer to the RX Family Software Manual.