< Assembler Command Options / List Options >
[Format]
If this option is not specified, no assemble list file is output.
[Description]
- | When the listfile option is specified, an assemble list file is output. The name of the file can also be specified. |
- | <file name> should be specified according to the rules described in the Naming Files section. |
- | If <file name> is not specified in the listfile option, the source file name with the extension replaced with .lst is used as the source list file name. |