-show


< Assembler Command Options / List Options >

[Format]

-show=<sub>[,...]
      <sub>: { conditionals | definitions | expansions }

[Description]

-

This option specifies the contents of the list file to be output by the assembler. The following output types can be specified as <sub>.

Table 2.12

Output Types Specifiable for show Option

Output Type

Description

conditionals

The statements for which the specified condition is not satisfied in conditional assembly are also output to a source list file.

definitions

The information before replacement specified by .DEFINE is output to a source list file.

expansions

The macro expansion statements are output to a source list file.

 

-